The Professional's Source for Hard-To-Find Computer Parts
McAfee Secure sites help keep you safe from identity theft, credit card fraud, spyware, spam, viruses and online scams    
Advanced Search
  My Cart:   0 Items Quick Buy Log In   United States   [change]
Home   >   Custom Manufacturing   >   Custom Cables

Custom Cable Experience
StarTech.com leads the industry with our outstanding selection of cables, backed by quality construction and a renowned warranty. Now you can harness our expertise and quality to design specialized cabling solutions for your unique needs. Our experience shows - have a look below at some of the successful projects we have completed.

Have a custom project? Get Started with a custom quote.

View Our Other Custom Engineering capabilities

 

Royal Bank Pinpad cable

Challenge
To provide a reinforced pinpad cable that could withstand everyday use.

Solution
Using a coiled design, we provided a better quality cable than what was originally used. The coiled design we used offered more flexibility, reducing the damage caused by repetitively moving the pinpad. This in turn reduced replacement and breakdown costs, not to mention the inconvenience of downtime.

Dell Optiplex Cash Register Cable

Challenge
The original cables were situated in such a way as to prevent it from bending, due to a tight fit between the cash register and a nearby wall.

Solution
Based on a low profile VGA cable, we used a low profile molding that proved to be more resilient against unnecessary bends in the cable. This in turn saved the company the money that would have been required to replace the cable, or repair the equipment using the cable

SATA Latching Cables

Challenge
Design a SATA cable solution for a system builder. The customer was incurring high support costs due to hard drive cables working loose in shipping and from vibration when in use. They were forced to hot glue standard SATA cables to the drives to prevent vibration.

Solution
StarTech.com worked closely with the customer's engineering team to design and tool left angle SATA connectors that would fit snugly into the drives. In addition, a metal latching system was incorporated into the connectors to ensure that firm reliable data connections would be maintained.

McDonald’s Canada – Drive-thru cables

Challenge
The repeated stress of high-volume drive-thru transactions was causing POS (pin pad) cables to break down.

Two step solution

  1. We first built a metal, water-resistant box containing a circuit board and power indicator, that could be used to reduce the length of cable required, in turn eliminating some of the normal wear and tear.
  2. We then designed a custom molded, coiled cable that would be able to withstand constant, repeated tension.

McDonald’s Canada – Cash Register ‘Pigtails’

Challenge
After updating their cash registers, the standard RS232 to RJ45 adapters used prior to the update could no longer be used to connect POS terminals to the main computer network.

Additional factors
Space limitations required a small form factor, due to the intended location.

Solution
We built custom RS232 to RJ45 “pigtails”, with low profile connectors, offering compatibility while maintaining a small footprint

Loblaw’s – POS Scanner Cable

Challenge
Electromagnetic interference created by checkout line conveyor belts was causing data scanning errors

Solution
We built a strong, yet flexible cable able to resist interference, comprised of custom wire and shielding, as well as strain relief molding to combat damage due to repeated use.

Shielded Cables for Healthcare


Challenge
Design and build completely shielded, medical grade cables for use in hospital environment. These cables carry critical patient data.

Solution
We custom engineered cables using completely shielded wire and connectors that solved previous interference issues.

Custom Molded Internal Data Cables


Challenge
A Global provider of IT security solutions required custom internal cables for use in digital video management system.

Solution
After thorough engineering engagement, we crafted custom molded connectors that met all color coding and labeling requirements.

Security Cable


Challenge
To provide a cable harness for internal use in proprietary closed circuit video equipment, that allowed for quick and fool-proof installation and replacement in the field.

Solution
Custom cut and zip tied wiring bundles were used with the required IDC type connectors, creating a single, compact and easily installable harness. Color coded wire and clearly labeled connectors were provided to ensure error free installation.

USB Digital


Challenge
Create a cable that would provide an internal USB type ‘A’ connection for a custom control module, that would terminate in an external molded USB type ‘B’ connector. It was critical that the cable be able to withstand the strain that would result from repeated usage and re-positioning.

Solution
We designed and prototyped a strongly shielded USB A-B cable, that would lock perfectly into the groove in the customer’s molded enclosure. Custom strain reliefs were then molded to fit on the inner and outer surfaces of the enclosure, ensuring that the cable would remain securely positioned while still allowing complete flexibility. The look and feel of the finished product were enhanced by the inclusion of the customer’s logo on the cable molding.

High Tech Hydra Cable


Challenge
Design a cable that would provide a high quality connection between a specialized digital projection device and a proprietary PCB, while minimizing the cable footprint, providing optimum durability and ease of installation. Other factors to consider included resistance to cable strain and potential signal degradation.

Solution
We engineered a cable that combined easily identifiable connectors, including RCA and minijack A/V, PS/2 keyboard and two RS-232 serial data lines into a single, optimally shielded harness. Due to the length and combined weight of the assembly, specially sourced thin gauge wire was used, and bundled within a molded PVC jacket to provide a lightweight, compact product at a very competitive cost.