The Professional's Source for Hard-To-Find Computer Parts
McAfee Secure sites help keep you safe from identity theft, credit card fraud, spyware, spam, viruses and online scams    
 
Advanced Search
  My Cart:   0 Items Quick Buy Log In   United States   [change]
Home   >   Tools & Guides   >   StarTech University   >   Specialized Cables
 
 
Course 4: Specialized Cables


Introduction

The term "cable" refers to a physical apparatus that is used to carry an electrical or communication signal from one device to another; although this basic function is identical among all cables, cables are often defined based on several other characteristics that distinguish them from one another.

For example:

  • The main function of the cable (e.g. "video cable, audio cable, KVM Cable)
  • The conductive material used inside the cable to carry the signal (e.g. copper, aluminum etc.)
  • The type of jacket material used to bundle the internal wire(s) that are used to carry the necessary signal
  • The type of insulation used within the cable
  • The manner in which the conductive material is arranged within the jacket
Types of Cables StarTech.com Offers:
Custom Cables
USB Cables
Networking Cables
Video/Monitor Cables
Internal PC Cables and I/O BackPlates
IEEE-1394 FireWire Cables
Audio & Game Cables
StarView/KVM Cables
Multiport Extension Cables
External Power Cables
Printer Cables
Keyboard/Mouse Cables
Serial/Parallel Peripheral Cables
Modem Cables
Gender Changers and Adapters
Telephone Cables/Adapters
SCSI Cables
SCSI Terminators
Data Switches/Switchboxes
Bulk Wire and Connectors
Flat Panel Monitor Cables
Structured Wiring

Next – Chapter 2 - Connectors & Conductors
Chapters

Chapter 1 - Introduction

Chapter 2 - Connectors & Conductors

Chapter 3 - Jackets & Insulation

Chapter 4 - Specialized Cables

Final Exam