The Professional's Source for Hard-To-Find Computer Parts
McAfee Secure sites help keep you safe from identity theft, credit card fraud, spyware, spam, viruses and online scams    
Advanced Search
  My Cart:   0 Items Quick Buy Log In   United States   [change]
Home   >   Tools & Guides   >   StarTech University   >   Hard to Find Computer Parts
 
 
Course 1: Hard to Find Computer Parts


Applications and types of hard-to-find parts

Here are some examples of how “hard to find” parts can help bridge gaps between legacy and cutting edge systems.

I/O cards
Most modern motherboards have been designed without ports that were available in previous versions. For example, it can be difficult to find a motherboard that offers new technology, such as a PCI Express interface as well as a serial or parallel port. It is not difficult, however, to find a motherboard that supports both PCI Express and PCI, therefore allowing the PCI slot to be used to add different interface capabilities.
Adapters/converters
Adapters and converters that bridge technologies are often times a very valuable addition to a computer system, specifically due to the cost-effectiveness and convenience that they provide. Some examples:

USB to PS/2 adapter – KVM specific (PS2TOUSB):

Although this product can be used with an end user computer system, it is used to separate a combined USB mouse and keyboard signal into two distinct signals – a PS/2 mouse signal, and a PS/2 keyboard signal. Because most KVM Switches use PS2 internal circuitry, they are incapable of using two signals from a single USB port, therefore recognizing only one of the devices.

USB to PS/2 adapter (GC46FMKEY, GC46FM):
  • Provides user with options as to how Mouse and Keyboard are connected
  • Frees up USB ports that could be better used for other devices such as digital cameras, printers etc.

IDE to Serial ATA Drive Motherboard Adapter (PATA2SATA):
  • Cost-effective – Allows proactive upgrade to SATA standard without having to upgrade the motherboard
  • Provides additional SATA connectivity, in place of IDE
  • Offers “forward compatibility”(“future-proofing”), as the SATA drive can be used with subsequent motherboard installations

Power adapters (CPUFANADAPT, LP4SATAFM, SATAPOWADAP):
Finding a power supply with the necessary component connections can sometimes be difficult. For example, a computer requires a new power supply (due to normal longevity and wear and tear), but everything else in the computer is working perfectly. It would be somewhat unorthodox to replace the contents of the computer, simply because a power supply has been exchanged.

Power adapters:
  • Provide cost-effective way to broaden connection compatibility
  • Reduce criteria for power supply purchasing decisions (i.e. connector types don’t need to prohibit a user from buying a less expensive power supply, as an adapter can be used in place)
  • Makes use of an otherwise unused connection


Next – Final Exam
Chapters

Chapter 1 - What makes a part "hard to find"?

Chapter 2 - If it isn’t Broken, Why Fix It!

Chapter 3 - The Importance of Hard-to-Find Parts

Chapter 4 - Applications and Types of Hard-to-find Parts

Final Exam