The Professional's Source for Hard-To-Find Computer Parts
McAfee Secure sites help keep you safe from identity theft, credit card fraud, spyware, spam, viruses and online scams    
Advanced Search
  My Cart:   0 Items Quick Buy Log In   United States   [change]
Home   >   Tools & Guides   >   StarTech University   >   SCSI School
 
 
Course 2: SCSI School


SCSI Types & Specifications

The following table illustrates the evolution and capabilities of the various permutations of SCSI technology, as determined by the following criteria:
For further clarification, please refer to the following definitions:

Interface: In this case, referring to a hardware interface – the physical connection between two pieces of hardware. For example, a USB keyboard connects peripherally to a host computer via the USB interface.

Throughput: A measurement used to identify the amount of data that can be transferred from one device to another, in a specified amount of time, typically measured in KB/s, MB/s etc.

Bus Width: A measurement used to determine the amount of data transmission, of which a device is capable. For example, a device with an 8-bit bus width can transmit 8 bits of data simultaneously, while a 32-bit device can concurrently transmit 32 bits of data per second.

Clock Speed: The speed at which a device can execute instructions, typically measured in MHz or GHz.

Maximum Number of Devices: The number of devices that can simultaneously be controlled from a single (in this case SCSI) interface.



Next – Chapter 6 - Rules for connecting SCSI devices
Chapters

Chapter 1 - What is SCSI?

Chapter 2 - SCSI vs. IDE

Chapter 3 - What is an SCA/RAID connector?

Chapter 4 - SCSI Signals

Chapter 5 - SCSI Types & Specifications

Chapter 6 - Rules for connecting SCSI devices

Chapter 7 - The Future of SCSI

Chapter 8 - SCSI Products

Final Exam