Upgrade to USB 3.0 Superspeed Connectivity
We've had some previous posts which outlined the benefits of the USB 3.0 connection for USB based peripherals. Benefits such as data transfer rates up to 5Gbs, making connectivity much quicker and more productive. Another key advantage of USB 3.0 is that it's backward compatible with all legacy USB 2.0 and 1.0/1.2 devices, which means adding USB 3.0 support will support existing peripherals, even if the ports aren't put to use with USB 3.0 products.
How do you ensure support? It’s simple really! If you have an available PCI Expansion slot, all you need is our latest expansion card, the PEXUSB3S2E2I; a 4 Port USB 3.0 PCI Express PCIe Controller Card. The PEXUSB3S2E2I gives users 2 external USB 3.0 ports, as well as 2 internal motherboard headers for internal or front mounted USB 3.0 devices.
It’s a versatile solution for supporting common USB 3.0 devices, as well as systems requiring internal USB 3.0 connections. As a forward compatible solution, this card offers a great way to increase productivity and adapt to the new standard!
comments powered by Disqus © 1985 - 2013 Copyright StarTech.com – All rights reserved.
Terms | Privacy
| SiteFeedback
RSS Feed
Follow us on Twitter | Find us on Google+