FOR IMMEDIATE RELEASE: JUNE 14, 2012

New HDMI®/HDMI® Micro to VGA Adapter Enables Users to Connect HDMI/HDMI Micro-equipped Smart Phones or Tablet Computers to a VGA Monitor/Projector

Video adapter saves the users the expense of upgrading existing displays by connecting tablets or smartphones to a VGA monitor or projector, supporting resolutions up to 1080p

Lockbourne, OH – June 12, 2012 - StarTech.com, a leading manufacturer of hard-to-find connectivity parts has announced the release of the MCHD2VGA – an HDMI®/HDMI® Micro to VGA Adapter, which enables users to connect an HDMI or HDMI Micro-equipped mobile device, such as a tablet computer or Smartphone to a VGA display or projector. The adapter provides a convenient and cost-effective alternative for users who need to integrate their mobile multimedia source to existing display devices, eliminating the expense of equipment upgrades.

The HDMI/HDMI Micro to VGA adapter includes an HDMI to HDMI Micro cable required for connecting HDMI Micro devices to the adapter which interfaces with the VGA display/projector. The adapter supports full 1080p output, which allows users to suitably display their high-definition or high-resolution content, as it was meant to be shown.

“The HDMI to HDMI Micro Adapter is the perfect solution for connecting your mobile HDMI-enabled devices to a VGA display or projector, especially users who are on the go who may not want to carry a full-sized laptop to do a presentation” said John Mardinly, Senior Product Manager for StarTech.com’s Audio-Video product line. “The product is compactly designed and is very light, which makes it easy to carry, and it includes a USB power adapter for scenarios where the mobile device is not able to output power.”

Features of the new HDMI to VGA Adapter include:

  • Includes HDMI to HDMI Micro Cable, for connecting to mobile HDMI devices
  • Supports a maximum resolution of 1920x1080 (1080p)
  • Includes an AC to USB Wall Adapter (required for use with HDMI Micro-equipped mobile devices, such as smartphones and tablet computers)

The MCHD2VGA HDMI®/HDMI® Micro to VGA Adapter is available for purchase from leading technology resellers including CDW, Newegg.com, Amazon.com, Tiger Direct, PC Connection, and Insight and will also be distributed by Ingram Micro, SYNNEX, D&H and Tech Data. MSRP for this product is $78.99 (USD) in the United States and $80.99 (CDN) in Canada.

For more information about this announcement, please contact Andrew Stephen at 1-800-265-1844 ext. 1248 or astephen@startech.com.

About StarTech.com

StarTech.com is an ISO 9001:2000 Registered manufacturer of hard-to find connectivity parts including A/V products, computer parts, cables and server management solutions. Founded in 1985, StarTech.com has locations in the United States, Canada, The United Kingdom, Europe and Taiwan, servicing a worldwide market.

View all press articles...

Year