StarTech.com’s New Universal Laptop Docking Stations Provide High Performance Workstation Connectivity for Hot Desking and Hotelling

Versatile dock adds multiple SuperSpeed USB 3.0, high speed Gigabit LAN and high quality display adapter ports, along with audio connections, to create an efficient multi-purpose or shared desk space

Lockbourne, OH - July 22, 2013 - StarTech.com, a leading manufacturer of hard-to-find connectivity parts, has announced the release of a new USB 3.0 Laptop Docking Station (USB3SDOCKHDV), which enables users to add HDMI and DVI-D, or HDMI and VGA dual video, as well as audio and Gigabit Ethernet connections to a laptop through a single USB 3.0 port.

The universal docking station allows laptops and Ultrabooks to be connected to peripherals such as monitors, keyboards and mice through a single USB port unlike manufacturer-specific laptop docks, which require that users’ laptops connect through a proprietary dock connector. This release adds to StarTech.com’s broad range of universal laptop docking stations, which provide users with an efficient and convenient way to transition between a fully mobile environment and a static workstation, especially in the case of workplaces that rely on hot-desking or hotelling desk space.

“This latest universal docking station significantly expands the functionality and connectivity of a desktop-stationed laptop or UltraBook, while taking advantage of the latest connectivity technologies” said Carey Cline, Senior Product Manager for StarTech.com’s Laptop Accessories product line. “Our laptop docks make it much easier for users to connect their laptop to the peripheral devices they need, without the disruption of having to connect multiple cables”.

Features of the USB3SDOCKHDV USB 3.0 laptop docking station include:

  • Dual display connectivity: HDMI and DVI-D or HDMI and VGA
  • Supports HD resolutions on both connected displays
  • Additional USB 3.0 hub ports
  • 10/100/1000 Mbps compatible RJ45 Ethernet port
  • Speaker and Microphone support via 3.5mm stereo mini-jacks
  • Supports the Windows® Aero® interface
  • Kensington Security Slot

MSRP for StarTech.com’s USB3SDOCKHDV Laptop Docking Station is $171.99 (USD) in the United States, $176.99 (CAN) in Canada and £143.99 (GBP exc. VAT) in the UK. The adapter is available from leading technology resellers including CDW, Newegg.com, Amazon.com, PC Connection, and Insight and will also be distributed by Ingram Micro, Tech Data, D&H, SYNNEX and ASI.

To learn more about StarTech.com’s USB3SDOCKHDV Laptop Docking Station, please visit www.StarTech.com/USB3SDOCKHDV. For more questions about this announcement, please contact Andrew Stephen at 1-800-265-1844 ext. 1248 or astephen@startech.com.

About StarTech.com
StarTech.com is an ISO 9001:2000 registered manufacturer of hard-to find connectivity parts including A/V products, computer parts, cables and server management solutions. Founded in 1985, StarTech.com has locations in the United States, Canada, Mexico, The United Kingdom, Europe and Taiwan, servicing a worldwide market.

View all press articles...