Support

Product FAQs


How do I enable the Read Error Skip feature of this duplicator?

You can use the SATDUP13 to skip bad sectors on a hard drive. For more information, visit the following FAQ: http://www.startech.com/ca/faq/hard_drive_duplicators_failing_drives.

To use the SATDUP13 to skip bad sectors, you need to enable Read Error Skip. By default, Read Error Skip is disabled.

To enable Read Error Skip, complete the following:

  1. Turn on the SATDUP13.

  2. Press ESC.

  3. Navigate to Setup and press OK.

  4. Navigate to Skip Error and press OK.

  5. Select the amount of sectors that you want to skip and press OK.

  6. To return to the duplication menu, press ESC and navigate to Copy.