Support

Product FAQs


How do I set up my Mini DisplayPort KVM switch?

  1. Turn off all of the computers and monitors that will be connected to the KVM switch.
  2. Connect the power adapter to the KVM switch. 
  3. Connect the Mini DisplayPort cable to your monitor and to the console Mini DisplayPort port on the KVM switch.
  4. Turn on the monitor.
  5. Connect your keyboard and mouse to the console PS/2 or USB ports on the KVM switch.
  6. If you have not done so already, change the KVM switch to focus on port 1.
  7. Connect the Mini DisplayPort cable to PC1 and to the KVM switch.
  8. Connect the PS/2 or USB cables to PC1 and to the PC1 PS/2 or USB ports on the KVM switch.
  9. Turn on PC1. The computer should load the operating system that you are using on PC1.
  10. Make sure that the mouse and keyboard can control PC1.
  11. Repeat steps 4 to 8 for each additional computer that you want to connect to the KVM switch. Leave the computer in focus until you make sure that the mouse and keyboard can control the computer.