Support

Product FAQs


How do I install my fax modem in Windows Vista / 7 / 8? (.exe method)

Note: In Windows 8 and 8.1 the device may auto-install.  For more information refer to the following FAQ: http://www.startech.com/faq/lsi_install_windows_8_8.1

Prior to installing this device, ensure that your operating system is up to date (for example, you have installed the most recent service pack).

To install the driver:

  1. Download the latest drivers from the StarTech.com website (http://www.startech.com/Support). You can find the part number and product ID on the product’s packaging.

Note: Windows will typically save the files to the Downloads folder that is associated with your user account (for example, C:\Users\your_name\Downloads).

  1. Once the download is complete, right-click the zip folder that you downloaded, select Extract All, and follow the on-screen instructions.
  2. In the list of extracted files, right-click the Setup.exe file and select Run as Administrator.

Note: If the Run as Administrator option is not available, you might be attempting to run the installer from within the zipped file. Extract the files using the instructions in Step 2.

  1. Follow the on-screen prompts to install the device drivers and restart the computer when prompted.
  2. Once Windows has restarted, connect the fax modem to your computer.
  3. Your computer will automatically complete the driver installation and your device should be ready to use.