Support

Product FAQs

Before You Buy

How can I tell if I can use this PS/2 USB adapter with my mouse or keyboard?

Passively converting from PS/2 to USB or USB to PS/2 is only possible with mice and keyboards that are compatible with both PS/2 and USB connections. The following are two ways to determine if these products will work for you:

  • Look on the bottom of your mouse or keyboard for a PS/2 symbol or picture, and a USB symbol or picture.
  • Your mouse or keyboard came with a similar PS/2 to USB or USB to PS/2 adapter.

You can use the USBPS2PC to actively convert PS/2 keyboards and mice to USB.

Note: StarTech.com PS/2 adapters are only officially supported by mice and keyboards.