Support

Product FAQs


What do I do if I am not achieving USB 3.1 speeds with my USB 3.1 device?

If your setup components support USB 3.1 but you are experiencing slower transfer speeds than you expected, consider the following:

  • A USB host connection with multiple USB 3.1 ports might not be able to support 10Gbps on each port simultaneously.
  • The type of port on a device does not determine whether the device is capable of USB 3.1 speeds. A USB-C port might not support USB 3.1 speeds, while USB-A and USB-B ports might support USB 3.1 speeds.
  • Any other devices that you include in your setup, such as an older hard drive in a USB 3.1 enclosure, might create a point of congestion and slow down transfer speeds.

To confirm the functionality of your USB host connection, its ports, and any other devices in your setup, refer to the information provided by the manufacturer.

Note: USB 3.1 is also known as USB 3.1 Gen 2 (10Gbps). Devices that support USB 3.1 should have the USB 3.1 symbol on them. If the USB 3.1 symbol does not appear on your USB source or device, refer to the information provided by the manufacturer to confirm whether the USB source or device support USB 3.1.