Support

Product FAQs


How do I reset my device to the default factory settings?

To perform a factory reset, press and hold the Reset button for 10 seconds.

To perform a factory reset through the web interface, perform the following:

  1. Make sure that the WFRAP433ACD is on the same network as your computer.
  2. In an Internet browser, enter the IP address of the unit. The default IP address is 192.168.10.1.
  3. In the user name field, enter the user name. The default user name is admin.
  4. In the password field, enter the password. The default password is admin.
  5. Under the Management section, click Save/Reload settings.
  6. Click Load default.