Some cookies are essential to ensure our website works for you. You may block or delete all cookies from this site but parts of the site may not work. To find out more about how we use cookies, see our privacy statement.
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
Low Profile Card

 

 

The Low Profile card allows for the design of a small, low profile system that still offers benefits in upgradeability and expandability to the user. There are two main card lengths (MD1 and MD2) that are defined for low profile PCI cards; MD1 is the shortest 32-bit card length available at 4.72", MD2 is the largest 32-bit card length available at 6".