Support

Product FAQs

Troubleshooting

How do I access this device’s web interface?

  1. Make sure that the NETRS232485 is on the same network as your computer.
  2. In an Internet browser, enter the IP address of the unit. The default IP address is 192.168.10.2.