Support

Product FAQs


I'm having difficulty setting my WIFI2VGA into STA mode, what do I do?

Some network equipment may cause a conflict with the WIFI2VGA, preventing the device from entering STA mode. If you're having difficulty setting the WIFI2VGA into STA mode, try the work around method below:

  1. Set the device into STA mode as per the Wireless Network Configuration section of the instruction manual.
  2. While the device is showing the "Configuring Network" message on the monitor connected to the device, unplug the network cable from the WIFI2VGA.
  3. Once back to the "Ready" screen, if it is not showing as being in STA mode, power off the device wait 5 seconds and power it back on.

Once it shows STA mode on the ready screen, run the PC2TV software again.