Support

Product FAQs


How do I mirror my primary display onto my secondary display in Windows?

Windows 10 / 8

  1. On your keyboard, press the Windows Key + X and select Control Panel.
  2. Click Appearance and Personalization, then click Display.
  3. Click the Resolution or Adjust Resolution option from the left column.
  4. Expand the drop-down menu next to “Multiple displays” and select Duplicate these Displays.
  5. Click OK to apply the changes and close the window.

Windows 7 / Vista

  1. Click the Start button and select Control Panel.
  2. Click Appearance and Personalization, then click Display.
  3. Click the Resolution or Adjust Resolution option from the left column.
  4. Expand the drop-down menu next to “Multiple displays” and select Duplicate these Displays.
  5. Click OK to apply the changes and close the window.

Windows XP

  1. Click the Start button and select Control Panel.
  2. Double-click Display.
  3. Click the Settings tab.
  4. Un-check the box beside Extend my Windows desktop onto this monitor.
  5. Click OK to apply the changes and close the window.