Support

Product FAQs


How do I change my IP address in Android OS?

  1. Tap the Settings app.
  2. Tap Wi-Fi.
  3. Touch and hold the network that you want to set the IP address for.
  4. Tap Manage network settings.

Note: Depending on the type of smartphone you are using and the version of the Android OS you are running, the text you see in step 4 might differ from Manage network settings.

  1. Select the Show advanced options check box.
  2. Under IP settings, tap the drop-down box.
  3. Tap Static.
  4. Enter the new IP address.
  5. If necessary, repeat step 8 for the gateway.
  6. Tap Save.

To change your IP address so that you can access a specific device, complete steps 1 to 6, then tap DHCP to access the Internet again.