Support

Product FAQs


Can I use the Ethernet port on my print server to connect to an Ethernet port on my printer?

The Ethernet port on a wireless network print server is intended to be used for configuration and to connect to an existing network infrastructure. You cannot connect an Ethernet port on a wireless network print server to the Ethernet port on a printer. The only supported method of connecting a printer to the print server is to use a USB A to B cable. These cables can be found on StarTech.com, in the USB 2.0 Cables section.