Support

Product FAQs


How do I access the web interface of my network serial device?

  1. Make sure that the computer is on the same network as the NETRS2322P. 
  2. In an Internet browser, enter the IP address of the unit. The default IP address is 192.168.1.40.
  3. Click Login