Support

Product FAQs


How do I access this device’s web interface?

  1. Make sure that the serial device is on the same network as your computer.
  2. In an Internet browser, enter the IP address of the unit. The default IP address is 192.168.0.35.
  3. In the password field, enter the password. The default password is admin.
  4. Click Configure.