Support

Product FAQs


How do I install my video capture card in Windows Vista / 7? (.exe method)

Before you install the device, make sure that your operating system is current (for example, the most recent service pack is installed).

  1. Navigate to http://www.startech.com/Support and download the latest software. The part number is USB2HDCAPS.

Note: Windows usually saves the files to the Downloads folder that is associated with your user account (for example, C:\Users\your_name\Downloads).

  1. When the download is complete, right-click the zip folder that you downloaded, select Extract All, and follow the on-screen instructions.
  2. In the list of extracted files, right-click the setup.exe file and select Run as Administrator.

Note: If the Run as Administrator option is not available, you might be attempting to run the installer from within the zipped file. Extract the files using the instructions in step 2.

  1. Follow the on-screen instructions to install the software.

When the software finishes downloading, it will be ready to use.