Support

Product FAQs


The monitor is not getting a signal and the monitor says “Out of Range.” What do I do?

The error “Out of Range” normally means that the resolution being output by the computer is not compatible with the display. Try lowering the resolution to see if that helps resolve the issue.  You may need to connect another monitor or restart the computer or source to accomplish this.