Support

Product FAQs

Installatie

How do I install my SVID2USB2 in Windows XP? (.exe method)

Prior to installing this device, ensure that your operating system is up to date (for example, you have installed the most recent service pack). Also, ensure that the USB 2.0 host driver is updated according to the latest version available.

To install the driver:

  1. Download the latest drivers from the StarTech.com website (http://www.startech.com/Support). You can find the part number and product ID on the product’s packaging.

Note: Windows will typically save the files to the Downloads folder that is associated with your user account (for example, C:\Documents and Settings\your_name\My Documents\Downloads).

  1. Once the download is complete, right-click the zip folder that you downloaded, select Extract All, and follow the on-screen instructions.
  2. Open the Driver folder.
  3. Double-click the Setup.exe file.
  4. Follow the on-screen prompts to install the device drivers and restart the computer when prompted.
  5. Once Windows has restarted, connect the video capture card to your computer.
  6. Your computer will automatically complete the driver installation.

To verify that the driver installed correctly:

  1. Press Windows Key + R, type devmgmt.msc, and click OK.
  2. Expand the Sound, video and game controllers section and verify that both devices are listed (USB EMP Audio Device for audio and USB 2821 Device for video).

To install the GrabBee software:

  1. In the list of extracted files from the download, open the SVID2USB2xx folder.
  2. Navigate to the GrabBee_V1.0.9.6 folder.
  3. Double-click the Setup.exe file.
  4. Follow the on-screen prompts to install GrabBee and restart the computer when prompted.
  5. *North American users only: In the options for GrabBee, set the Video Format to NTSC-M. For more information, visit the StarTech.com website to see the SVID2USB2 manual. It is available under the Drivers & Downloads tab for the SVID2USB2.