Support

Product FAQs

Voor uw aanschaf

Are there any USB controllers that have a known incompatibility with this USB3HDCAP?

There are known USB controller incompatibilities between the USB3HDCAP capture card and ASMedia and Etron USB controller cards. Intel, AMD, Renesas, and Via, are some of the USB controllers that are confirmed to work with the USB3HDCAP capture card.

Note: When you use a Via USB controller, you may need to get the drivers from Via's website instead of using the drivers that are automatically installed during Windows Update.

If your computer only has ASMedia or Etron USB controllers, you can add a USB 3.0 expansion card to your desktop or laptop to work around this issue.

To check which USB controller you have on a computer running Windows, complete the following:

  1. Press the Windows key + R.
  2. Type devmgmt.msc and click OK.
  3. In Device Manager, click the arrow or plus sign next to USB Serial Bus controllers.
  4. In the list of USB controllers, look for any brands such as Intel, AMD, Renesas, Via, Etron, or ASMedia. In general the brands are listed as [Brand] Enhanced Host Controllers, or something similar to [Brand] USB 3.0 Host Controller or Root Hub.