Are you in the United States?
Visit our U.S.A. & International site for relevant pricing, distribution and product availability information.
Go to StarTech.comSlimline SATA to SATA Adapter with Power - F/M
Use new Slimline drives with older motherboards
Produkt ID: SLSATAADAP
- Compliant with Serial ATA III Specifications
Inte tillgängligt
Kan finnas hos partners
Från en partner
Support
Överblick
The SLSATAADAP Slimline SATA to SATA adapter is a cost-saving solution that allows you to connect a Slimline SATA optical drive to a standard SATA motherboard connection.
The adapter features a Slimline SATA connector on one side and a standard SATA data connector on the other; power is drawn through a power supply SATA power connector, combining both data and power into the optical drive Slimline SATA connection.
The Slimline SATA to Standard SATA adapter is backed by Lifetime Warranty and free lifetime technical support.
Fördelarna med StarTech.com
- Cost-effective way to connect a Slimline SATA optical drive to a standard SATA motherboard using standard SATA cables
- Easy to use and install
- Backed by StarTech.com's lifetime warranty
Tekniska specifikationer
Produktnummer | ||
---|---|---|
Ingram Micro Sweden | V930889 | |
UPC Code | 065030835497 |
Information om garanti | ||
---|---|---|
Garanti | Lifetime | |
Hårdvara | ||
Kabelmanteltyp | PVC - Polyvinyl Chloride | |
Kontakt(er) | ||
Connector A | 1 - Slimline SATA (13-stifts, data & ström) Honuttag | |
Connector B | 1 - SATA data- & ström-kombo (7+15-stifts) Kontakt | |
Utseende | ||
Produktbredd | 11 mm [0.4 in] | |
Produkthöjd | 8 mm [0.3 in] | |
Produktlängd | 46.1 mm [1.8 in] | |
Produktvikt | 33.6 g [1.2 oz] | |
Förpackning | ||
Fraktvikt (förpackning) | 0.1 kg [0.2 lb] | |
Vad det är i lådan | ||
Ingår i paketet | 1 - Slimline SATA to SATA Adapter with Power - F/M |
Relaterade produkter
6in Slimline SATA to SATA Adapter with Power - F/M
Connect a Slimline SATA optical drive up to 6in away from a standard SATA motherboard connection
Produktsupport
Drivrutiner & hämtningsbara filer
Compliance Letter(s):
Specifikation(er)
- SLSATAADAP_Datasheet-SV.pdf
Svenska
Vanliga frågor
Problemsökning
When you troubleshoot issues with a SATA cable, there are some quick tests that you can complete to rule out potential problems. You can test to make sure that the following components are working correctly and are not the source of the issue:
-
Hard disk drive
-
Hard drive controller (for example, motherboard)
-
SATA cable
To test your setup components, try the following:
-
Use the hard disk drive, hard drive controller, and SATA cable in another setup to see if the problem is with the components or the setup.
-
Use a different hard disk drive, hard drive controller, and SATA cable in your setup to see if the problem persists. Ideally, you should test a component that you know works in another setup.
When you test the hard disk drive, hard drive controller, and SATA cable, it is recommended that you do the following:
-
Make sure that the hard drive is spinning without the SATA cable attached. The power cable should make the drive spin if it is a mechanical drive and not a solid state drive.
-
If your operating system is not detecting the hard disk drive, make sure that the drive is formatted with a partition (for example, NTFS or FAT32). If you are using a computer running a version of Windows, a drive letter must also be assigned to the hard disk drive.
For more information about how to initialize a drive, refer to the following FAQ: https://www.startech.com/support/faqs/technical-support?topic=hard-drives#initialize-hard-drives.
Copy Link
Was this information helpful? Ja Nej
* Produkters utseende och specifikationer kan komma att ändras utan förvarning.