Support

Product FAQs

Problemsökning

How do I set up or change the RAID mode for my hard drive enclosure?

Note: Any data currently on the drives will be lost during this process. You need to back up all of your data before you set a RAID mode.

The hard drive enclosure must have a RAID mode set before you can use it. To set or change a RAID mode, complete the following:

  1. If the power adapter is not plugged in, plug it in.
  2. Turn off the hard drive enclosure.
  3. Change the DIP switches to match the RAID mode that you want to set.
  4. Press the Reset button.
  5. Turn on the hard drive enclosure.