Support

Product FAQs

Problemsökning

Only the monitors hooked up through VGA or hooked up through DVI are working. What do I do?

This KVM switch is meant to be used with two monitors, with up to two or four computers, each with an available VGA and DVI port. 

The VGA ports on the KVM switch only talk to each other, and the DVI ports work in the same way. Therefore, if you plug a VGA monitor into the KVM switch and only plug a DVI cable into your computer, your monitor will not work.