Product FAQs

Hur man

How do I ping another network device to make sure that they can see each other in Windows?

You can use the ping command to verify the connectivity between two network devices that are IP (Internet Protocol) based.

To ping another network device using a computer running Windows, complete the following:

  1. To bring up the run dialog, press the Windows key + R.
  2. Type cmd and press Enter.
  3. Type ping <IP address> and press Enter. The IP address is XXX.XXX.XXX.XXX, where XXX is a number between 0 and 255. For example, to ping, you would type ping

If the ping is successful, you should receive replies from the address that you are trying to ping. If the ping is unsuccessful, you need to diagnose your network setup further.

To verify if your local network adapter is working, you can ping, which is a loopback address. The loopback address is a virtual network port for most operating systems.