Product FAQs

Before You Buy

Are there any network requirements for the USB2HDCAPS?

In order for network streaming to work with ShareView, your network infrastructure must have a DHCP server included on the network. The DHCP server issues an IP address to the USB2HDCAPS and allows any computer on the same network running ShareView to discover the USB2HDCAPS.

When you use network streaming with the USB2HDCAPS, consider the following:

  • A static IP address cannot be set.

  • Only a 10/100 connection is required.

  • only supports the use of ShareView software for network streaming and does not support the use of third-party streaming software.