New USB-C Docking Station Features Power Delivery

First USB-C™ docking station utilizes speed, bandwidth and power delivery from USB-C technology.

Lockbourne, OH - August 16, 2016 - has announced the release of a USB-C Dual Monitor Docking Station with Power Delivery (SKU: MST30C2DPPD), for availability in late August. This is one of the first USB-C Dual Monitor Docking Stations on the market to incorporate USB-C technology with power delivery.

The dock is a simple solution for turning a USB-C enabled laptop, such as the Dell XPS™ or Chromebook Pixel™, into a productive full-scale workstation. The dock supports full power delivery to the laptop and the devices connected to it, only the dock’s power adapter is needed to power the laptop and devices, eliminating the need to have a power adapter for each device. With MST technology enabled, the laptop screen can be expanded to two DisplayPort monitors, creating a more productive workstation.

Business professionals, IT departments or any USB-C laptop user will find this docking station to be beneficial for multi-user workstations and hot desk environments. Users connect their USB-C laptops to additional peripherals and displays through a single cable, and this docking station provides additional ports for charging, network access and audio.

Additional features of the USB-C docking station are:

  • 60w power delivery for charging laptops and powering other devices
  • Single 4K DisplayPort or HDMI video output
  • Dual 2K video support for HDMI and DisplayPort monitors
  • MST technology offers support for a DisplayPort daisy chain, to two separate monitors
  • Multiple USB 3.0 ports for connecting additional devices
  • A fast-charge and sync port for quickly charging a phone or other mobile devices
  • Gigabit Ethernet port to add a wired network
  • Small, compact footprint
“The first USB-C docking station from demonstrates our commitment to providing laptop accessory products that utilize the latest technology to deliver a solution that simplifies the user’s setup and maximizes performance close to a full workstation,” said Carey Cline, Senior Product Manager,

For more information on USB-C, please visit:

To view a full selection of docking stations, please visit:

The USB-C docking station will be available at CDW,,, PC Connection, and Insight and will be distributed by Ingram Micro, SYNNEX, Tech Data, D&H and ASI.

View all press articles...