Support

Product FAQs


Can I use my network card for a Preboot Execution Environment (PXE)?

StarTech.com does not support a Preboot Execution Environment (PXE) as this requires third-party software. However, our devices can be used as long as the following conditions are met:

  1. The BIOS must support PXE.
  2. The BIOS must see the card.
  3. The environment must have drivers for the chipset used in the card.
  4. If using a USB networking card, the environment must have support for USB devices as well.