Support

Product FAQs


How do I adjust the audio settings on this device?

To select the audio format that this device outputs, complete the following:

  1. Press the Menu button.
  2. Press + or to select Audio EDID.
  3. Press Menu.
  4. Press + or to select one of the following setting options:
  • LPCM
  • 2CH
  • LPCM 4CH
  • LPCM 8CH
  • BITSTREAM
  • HD
  1. Press Menu to apply the changes.