Like it or not, the way we think of the office has changed dramatically since 2020. For decades, the standard was a dedicated working space, likely a cubicle, specifically to your liking. In many workplaces, those days are gone; the office is different now. As we all continue to adapt to the new normal, offices worldwide are navigating how to create safe, functional, and collaborative working spaces for their teams to return to. This is where the concept of office or desk hoteling comes in. Hoteling, which differs from hot-desking, is the practice of having meeting rooms, working spaces, and desks reserved or booked in advance for an employee to use for some time. Hoteling isn't a new concept, it has been around for decades, but with the dramatic changes we have seen in the workplace while we figure out what normal is and how we will return to the office, this philosophy has gained a lot of tracking. Even here at StarTech.com, we are implementing office hoteling to allow our teams to get back to the office when needed and meet with their coworkers. One hurdle to clear with hoteling is how to design a workspace that will suit the diverse needs of your team. The work happening at a hotel desk on a Monday can be dramatically different on a Friday. Planning and the investment in the proper hardware and accessories are crucial to being successful. Read on to see how StarTech.com accessories can help you bring your team back to the office with enhanced productivity. Mounts and Ergonomics The first step in creating a productive and valuable hotel desk is proper ergonomics that can adjust to suit the needs of anyone on your team. StarTech.com offers a variety of single and multi-monitor mounts to help you optimize your space and increase productivity. Your hotel desks need to be versatile and accommodating for the varying needs of your team from day to day. Here are a few options to consider; A single or dual mount with USB 3.0 ports, providing your team with additional I/O ports such as our ARMPIVOT2USB3 or ARMSLIMDUOS. These mounts support displays sizes up to 32", offer 90-degree tilt, swivel and rotation and contain 2 USB 3.0 ports in the base of the mount. One of the advantages to working from home that many of us experienced was the ability to move around while we did our work. While moving around the office in the new normal may be limited, one option to increase ergonomics at your hotel workstation is opting for a sit-stand workstation. Our sit-stand mounts come in various configurations and can help your team stay comfortable throughout the day. Below is ours in action. Once you have the ergonomics and comfort sorted, you need to equip your team with proper I/O to be productive while using their hotel desk. While a traditional laptop docking station is ideal, the global chip shortage continues to have a widespread effect on inventory levels. However, a USB-C multiport adapter is an excellent alternative. It will save you valuable space in your office's hotel configuration. Multiport Adapters and Hubs As discussed, the challenge with desk hoteling is creating a workspace that meets everyone's needs. We offer a wide variety of USB-C multiport adapters offering all the ports and features needed. Find out which USB-C Multiport adapter is best for you or your team HERE. Our DKT30CHSDPD1 features 4K 60Hz HDR10 video, a 2-Port USB-A Hub at 5Gbps, USB Fast-Charging, 100W Power Delivery, SD + MicroSD Card Reader, and Gigabit Ethernet. This adapter and many other new StarTech.com multiport adapters also feature an extra-long 12" host cable, reducing cable and port strain producing a more durable and long-lasting product. Power and Charging Setting up a workstation 100% to your liking is a challenge with hoteling. Team members may end up over-preparing for their day by packing additional chargers and cables to avoid having their laptop or phone run out of battery mid-day. Save them the hassle of lugging these additional items to and from the office by equipping your workstations with a 60W USB-C laptop charger, a secure USB-C charging cable and a Qi wireless charging stand. Our WCH1C USB-C laptop charger will keep your team's devices topped up throughout the day while also offering valuable features such as over-voltage and short-circuit protection. Don't forget about the commute! StarTech.com has also recently launched its first-ever laptop backpacks. These backpacks were designed with the IT Pro in mind. The bags feature an innovative built-in IT Accessories Case keeping your connectivity accessories organized and easily accessible when you're on the go. On top of that, the backpacks are constructed out of a durable 1680D ballistic nylon and feature steel zippers. Available in 15" & 17" sizes, these backpacks are your new hybrid work companion! Check them out. Has your office started to transition to a hoteling model? Head over to our IT Pro Community and let us know what products you think are crucial to a productive office hoteling setup.