Will a passive DisplayPort adapter work with a Thunderbolt 3 docking station? Active adapters are required if adapting DisplayPort to HDMI or DVI monitors. Active adapters use additional chips to make the conversion inside the adapter. Passive DisplayPort to HDMI or DVI will not work with this device. Examples of active adapters: DP to HDMI: DP2HD4K60S DP to DVI: DP2DVIS DP to VGA: DP2VGA2 This FAQ applies to these products: TB3CDK2DP, TB3DK2DHV, TB3DK2DPM2, TB3DK2DPPD, TB3DK2DPW, TB3DKDPMAW, TB3DKM2DP, TB3DOCK2DPPD, USB3DDOCKFT