Support

Product FAQs

Common Issues

How can I check the IP address of my router?

Windows

The easiest way of determining the IP address of your router in Windows is to use the “ipconfig /all” command. The output of this command will display an IP address for “Default Gateway” - this is your router. To use this command, complete the following:

  1. Go to the Windows Desktop screen.
  2. Press the Windows key + R.
  3. Type cmd in the text field and press Enter.
  4. Type ipconfig /all.

Mac OS

The easiest way of determining the IP address of your router in Mac OS is to check Network settings. To find the IP address for your router, complete the following:

  1. Click on Apple menu.
  2. Click on System Preferences.
  3. Click on Network.
  4. Highlight the network being used, and click Advanced.
  5. Click the TCP/IP tab near the top of the window.

Your router's IP address is listed beside Router.