Support

Product FAQs

Problemsökning

How do I access this device’s web interface?

  1. Make sure that the IES101GP2SFW is on the same network as your computer.
  2. In an Internet browser, enter the IP address of the unit. The default IP address is 192.168.0.100.
  3. In the user name field, enter the user name. The default user name is admin.
  4. In the password field, enter the password. The default password is admin.