Support

Product FAQs

Problemsökning

How do I access this device’s web interface?

  1. Make sure that the IP KVM switch is on the same network as your computer.
  2. In an Internet browser, enter the IP address of the unit. If the IP KVM switch does not detect a DHCP server, the default IP address is 192.168.0.60.

Note: This device has Dynamic Host Configuration Protocol (DHCP) enabled by default, and will be assigned an IP address by your router when connected to your network. View the router's DHCP table to determine the IP address.