Support

Product FAQs

Problemsökning

My keyboard keeps repeating keys when it is plugged into the KVM. What do I do?

If the keys on your keyboard are repeating, complete the following:

  1. If the KVM you are using has USB ports, you can move your keyboard to the USB hub port on the back of the KVM (the USB hubs are marked).

Note: When you move the keyboard out of the keyboard port, you will not be able to access the hotkeys.

  1.  You can adjust the typematic rate in your operating system’s settings. Depending on the version of Windows you are running, you can adjust the typematic rate by doing one of the following:
    • Click Control Panel > Keyboard > Speed. Adjust the repeat delay and repeat rate until the keys no longer repeat.
    • Click Control Panel > Hardware and Sound > Devices and Printers. Right-click Keyboard Settings. Adjust the repeat delay and repeat rate until the keys no longer repeat.